AssociativeArcBuilderMidReference Enumeration

NXOpen.Features.AssociativeArcBuilder.MidReference is an alias for NXOpen.Features.AssociativeArcBuilderMidReference

class NXOpen.Features.AssociativeArcBuilderMidReference

Bases: object

Represents references for mid point

Enum Members

Enum Member Enum Member Description
Wcs
WCS
Absolute
Absolute CSYS
CordinatesSystem
CSYS
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.