AngularDimBuilder Class¶
-
class
NXOpen.Features.
AngularDimBuilder
¶ Bases:
NXOpen.Features.DimensionBuilder
Represents a
NXOpen.Features.AngularDim
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateAngularDimensionBuilder()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AlternativeAngle | Returns or sets the alternative angle toggle allows you to compute angle that is 360 degree subtracts current angle |
ComplementAngleFlag | Returns or sets the complement angle flag |
DimensionLocation | Returns the dimension location/placement controlled by the annotation origin block |
FaceChangeOverflowBehavior | Returns the face change overflow behavior. |
FacesToMove | Returns the faces being moved as part of the Linear Dimension command |
MeasurementObject | Returns the measurement object is for the move object |
OriginObject | Returns the origin object is for the fixed object |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SaveConstraints | Returns the SaveConstraints builder which is used by ADM Dimension Features. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Value | Returns the value of the dimension |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDimension | The drafting dimension which is used as UI tool for dimension display. |
GetFeature | Returns the feature currently being edited by this builder. |
GetIsComplementAngle | Returns the flag indicating if angle is complement @return the flag for complement angle |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetInterpartSourceEdge | Sets the interpart source edge |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AlternativeAngle¶
-
AngularDimBuilder.
AlternativeAngle
¶ Returns or sets the alternative angle toggle allows you to compute angle that is 360 degree subtracts current angle
-------------------------------------
Getter Method
Signature
AlternativeAngle()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AlternativeAngle(alternativeAngle)
Parameters: alternativeAngle (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
ComplementAngleFlag¶
-
AngularDimBuilder.
ComplementAngleFlag
¶ Returns or sets the complement angle flag
-------------------------------------
Getter Method
Signature
ComplementAngleFlag()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ComplementAngleFlag(complementAngleFlag)
Parameters: complementAngleFlag (bool) – New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
MeasurementObject¶
-
AngularDimBuilder.
MeasurementObject
¶ Returns the measurement object is for the move object
-------------------------------------
Getter Method
Signature
MeasurementObject()
Returns: Return type: NXOpen.SelectNXObject
New in version NX6.0.0.
License requirements: None.
OriginObject¶
-
AngularDimBuilder.
OriginObject
¶ Returns the origin object is for the fixed object
-------------------------------------
Getter Method
Signature
OriginObject()
Returns: Return type: NXOpen.SelectNXObject
New in version NX6.0.0.
License requirements: None.
Method Detail¶
GetIsComplementAngle¶
-
AngularDimBuilder.
GetIsComplementAngle
¶ Returns the flag indicating if angle is complement
Signature
GetIsComplementAngle(dimensionLocation)
Parameters: dimensionLocation ( NXOpen.Point3d
) – Indicates dimension origin cursor locationReturns: the flag for complement angle Return type: bool New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
SetInterpartSourceEdge¶
-
AngularDimBuilder.
SetInterpartSourceEdge
¶ Sets the interpart source edge
Signature
SetInterpartSourceEdge(interpartSourceEdge)
Parameters: interpartSourceEdge ( NXOpen.Edge
) – edgeNew in version NX8.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
AngularDimBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.