AnalyzePocketBuilderToolTypes Enumeration

NXOpen.Features.AnalyzePocketBuilder.ToolTypes is an alias for NXOpen.Features.AnalyzePocketBuilderToolTypes

class NXOpen.Features.AnalyzePocketBuilderToolTypes

Bases: object

Represents the tool type which defines how the angled walls are cut.

Enum Members

Enum Member Enum Member Description
Unknown
unknown.
EndMill
End Mill.
TCutter
T Cutter.
SphericalMill
Spherical Mill.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.