AestheticFaceBlendBuilderSegmentationType Enumeration

NXOpen.Features.AestheticFaceBlendBuilder.SegmentationType is an alias for NXOpen.Features.AestheticFaceBlendBuilderSegmentationType

class NXOpen.Features.AestheticFaceBlendBuilderSegmentationType

Bases: object

Segmentations options

Enum Members

Enum Member Enum Member Description
AtAllTransitions
Segmentation at all transitions
AtTransitionsonFaceChain1
Segmentation at Face Chain1 transition
AtTransitionsonFaceChain2
Segementation at Face Chain2 transition
AtAllTransitionsandMergeSmallBlendFaces
Secgmentation at all transitions and merge small blend faces
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.