AestheticFaceBlendBuilderRhoType Enumeration

NXOpen.Features.AestheticFaceBlendBuilder.RhoType is an alias for NXOpen.Features.AestheticFaceBlendBuilderRhoType

class NXOpen.Features.AestheticFaceBlendBuilderRhoType

Bases: object

Rho options

Enum Members

Enum Member Enum Member Description
Relative
Relative Rho: it’s the ratio of BaseRadius/(BaseRadius + CenterRadius)
Absolute
Absolute Rho: does not take into account the subtended angle
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.