AestheticFaceBlendBuilderCenterType Enumeration

NXOpen.Features.AestheticFaceBlendBuilder.CenterType is an alias for NXOpen.Features.AestheticFaceBlendBuilderCenterType

class NXOpen.Features.AestheticFaceBlendBuilderCenterType

Bases: object

Center methods will define peak of the blend

Enum Members

Enum Member Enum Member Description
CenterRadius
Center radius option.
Rho
Rho is the ratio of the center radius and the base radius.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.