AestheticFaceBlendBuilderBlendFacesType Enumeration

NXOpen.Features.AestheticFaceBlendBuilder.BlendFacesType is an alias for NXOpen.Features.AestheticFaceBlendBuilderBlendFacesType

class NXOpen.Features.AestheticFaceBlendBuilderBlendFacesType

Bases: object

Trimming options

Enum Members

Enum Member Enum Member Description
TrimtoAllInputFaces
Trims all input faces.
TrimtoShortInputFaces
Trims short input faces.
TrimtoLongInputFaces
Trims long input faces.
DoNotTrimBlendFaces
This option controls to trim blend faces or not
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.