AestheticFaceBlendBuilderAlignmentType Enumeration¶
NXOpen.Features.AestheticFaceBlendBuilder.AlignmentType is an alias for NXOpen.Features.AestheticFaceBlendBuilderAlignmentType
-
class
NXOpen.Features.
AestheticFaceBlendBuilderAlignmentType
¶ Bases:
object
Alignment method provides the ability to align the cross sections of the blend in the user specified direction
Enum Members
Enum Member Enum Member Description RollingBall Rolling Ball option will align the sections at contact point. SpineCurve Spine Curve option will align the sections based on a string of curves. Vector Vector option will align the sections based on the vector -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-