AeroRibBuilderGuideObjectTypes Enumeration

NXOpen.Features.AeroRibBuilder.GuideObjectTypes is an alias for NXOpen.Features.AeroRibBuilderGuideObjectTypes

class NXOpen.Features.AeroRibBuilderGuideObjectTypes

Bases: object

This attribute represents the Guide Object types

Enum Members

Enum Member Enum Member Description
Face
Guide object is face
DatumPlane
Guide object is datum plane
Curve
Guide object is curve
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.