AOCSBuilderOffsetType Enumeration

NXOpen.Features.AOCSBuilder.OffsetType is an alias for NXOpen.Features.AOCSBuilderOffsetType

class NXOpen.Features.AOCSBuilderOffsetType

Bases: object

AOCS builder offset type enum.

Enum Members

Enum Member Enum Member Description
Chordal
offset_type_chordal
Arclength
offset_type_arclength
Geodesic
offset_type_geodesic
Tangential
offset_type_tangential
Projectdistance
offset_type_projectdistance
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.