AOCSBuilderOffsetDistanceType Enumeration

NXOpen.Features.AOCSBuilder.OffsetDistanceType is an alias for NXOpen.Features.AOCSBuilderOffsetDistanceType

class NXOpen.Features.AOCSBuilderOffsetDistanceType

Bases: object

AOCS builder offset distance type enum.

Enum Members

Enum Member Enum Member Description
Constant
constant offset
Variable
variable offset
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.