SubdivideFacetBodyBuilderSubdivisionMethodType Enumeration

NXOpen.Facet.SubdivideFacetBodyBuilder.SubdivisionMethodType is an alias for NXOpen.Facet.SubdivideFacetBodyBuilderSubdivisionMethodType

class NXOpen.Facet.SubdivideFacetBodyBuilderSubdivisionMethodType

Bases: object

Subdivision methods

Enum Members

Enum Member Enum Member Description
SubdivideIntoFour
Subdivides the polygons into four sub triangles. The original mesh structure remains.
SubdividebyEdgeLength
Subdivides the polygons to a specified edge length. The original mesh structure disappears.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.