SubdivideFacetBodyBuilderInterpolationMethodType Enumeration¶
NXOpen.Facet.SubdivideFacetBodyBuilder.InterpolationMethodType is an alias for NXOpen.Facet.SubdivideFacetBodyBuilderInterpolationMethodType
-
class
NXOpen.Facet.
SubdivideFacetBodyBuilderInterpolationMethodType
¶ Bases:
object
Subdivision interpolation methods
Enum Members
Enum Member Enum Member Description Linear In the linear option the sub-triangles are coplanar to the original triangle. Shape resolution remains untouched.Cubic In the cubic option the sub-triangles are fitted cubic to the surrounding triangles. Shape resolution increases.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-