SewFacetBodyBuilderVertexIndex Enumeration

NXOpen.Facet.SewFacetBodyBuilder.VertexIndex is an alias for NXOpen.Facet.SewFacetBodyBuilderVertexIndex

class NXOpen.Facet.SewFacetBodyBuilderVertexIndex

Bases: object

Index of the vertex

Enum Members

Enum Member Enum Member Description
First
Index of the first vertex
Second
Index of the second vertex
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.