SewFacetBodyBuilderInput Enumeration¶
NXOpen.Facet.SewFacetBodyBuilder.Input is an alias for NXOpen.Facet.SewFacetBodyBuilderInput
-
class
NXOpen.Facet.
SewFacetBodyBuilderInput
¶ Bases:
object
Represents the option for keeping, deleting or hiding input two facet bodies after builder committing
Enum Members
Enum Member Enum Member Description Keep Keep the input facet body after builder committingDelete Delete the input facet body after builder committingHide Hide the input facet body after builder committing-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-