STLImportBuilderFacetBodyTypes Enumeration¶
NXOpen.Facet.STLImportBuilder.FacetBodyTypes is an alias for NXOpen.Facet.STLImportBuilderFacetBodyTypes
-
class
NXOpen.Facet.
STLImportBuilderFacetBodyTypes
¶ Bases:
object
These represent the type of body that will get created on importing the STL file
Enum Members
Enum Member Enum Member Description Nx Import To NX Facet FormatJt Import to JT formatPsm Import to Facet Brep format-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-