MergeFacetBodyBuilderInput Enumeration

NXOpen.Facet.MergeFacetBodyBuilder.Input is an alias for NXOpen.Facet.MergeFacetBodyBuilderInput

class NXOpen.Facet.MergeFacetBodyBuilderInput

Bases: object

Represents the option for keeping, deleting or hiding input two facet bodies after builder committing

Enum Members

Enum Member Enum Member Description
Keep
Keep the input facet body after builder committing
Delete
Delete the input facet body after builder committing
Hide
Hide the input facet body after builder committing
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.