FillHoleBuilderTargetTypes Enumeration

NXOpen.Facet.FillHoleBuilder.TargetTypes is an alias for NXOpen.Facet.FillHoleBuilderTargetTypes

class NXOpen.Facet.FillHoleBuilderTargetTypes

Bases: object

Options defining how to target holes for filling.

Enum Members

Enum Member Enum Member Description
UserDefined
Fills user-defined target holes.
ByNumberOfEdges
Automatically target holes based on number of edges.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.