FillHoleBuilderSmoothTypes Enumeration

NXOpen.Facet.FillHoleBuilder.SmoothTypes is an alias for NXOpen.Facet.FillHoleBuilderSmoothTypes

class NXOpen.Facet.FillHoleBuilderSmoothTypes

Bases: object

Smoothness and boundary continuity options.

Enum Members

Enum Member Enum Member Description
Linear
Linear (triangulated) fill.
Refined
Smooth internal fill.
TangentBased
Smooth fill, boundary is based on facet body tangent.
CurvatureBased
Smooth fill, boundary is based on facet body curvature.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.