FacetedFaceFacetedfaceType Enumeration

NXOpen.Facet.FacetedFace.FacetedfaceType is an alias for NXOpen.Facet.FacetedFaceFacetedfaceType

class NXOpen.Facet.FacetedFaceFacetedfaceType

Bases: object

Facet Face type

New in version NX8.5.1.

Enum Members

Enum Member Enum Member Description
Undefined
Undefined body type
Planar
Planar face
Cylindrical
Cylindrical face
Conical
Conical face
Spherical
Spherical face
Toroidal
Face from toroid
Parametric
Parametric face
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.