FacetedEdgeFacetededgeType Enumeration

NXOpen.Facet.FacetedEdge.FacetededgeType is an alias for NXOpen.Facet.FacetedEdgeFacetededgeType

class NXOpen.Facet.FacetedEdgeFacetededgeType

Bases: object

Facet Edge type

New in version NX8.5.1.

Enum Members

Enum Member Enum Member Description
Undefined
Linear
Linear edge
Circular
Circular edge
Elliptical
Elliptical edge
Intersection
Intersection edge
Spline
Spline edge
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.