CleanupFacetBodyBuilder Class¶
-
class
NXOpen.Facet.
CleanupFacetBodyBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Facet.CleanupFacetBodyBuilder
builder.It removes defects that are present in the surfaces of the bodies selected.
To create a new instance of this class, use
NXOpen.Facet.FacetModelingCollection.CreateCleanupFacetBodyBuilder()
Default values.
Property Value FoldedEdges Analyze InconsistentNormals Analyze LaminarSlits Analyze LongFacets Analyze MaxRatioLongFacets 10 MinAngleFoldedFacets 15 OriginalBodyOption Delete SelfIntersections Analyze ShowInfo 0 ThinFacets Analyze New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
FoldedEdges | Returns or sets the option to identify or repair facets having an angle with adjacent facets less than a specified minimum value |
InconsistentNormals | Returns or sets the option to identify or repair normals of neighboring facets or vertices that do not have the right orientation |
InputBodies | Returns the input facet bodies to be analyzed or repaired |
LaminarSlits | Returns or sets the option to identify or repair thin holes or slits in the mesh caused by facets not being aligned |
LongFacets | Returns or sets the option to identify or repair facets with a ratio of longest to shortest side exceeding a specified value |
MaxRatioLongFacets | Returns or sets the specified value used to define long facets |
MinAngleFoldedFacets | Returns or sets the minimum angle between adjacent facets to define folded facets |
OriginalBodyOption | Returns or sets the option for handling the input facet bodies |
SelfIntersections | Returns or sets the option to identify or repair facets of the same mesh intersecting each other |
ShowInfo | Returns or sets the option to display numbers of various type of defects identified or repaired in the NXOpen.ListingWindow . |
Tag | Returns the Tag for this object. |
ThinFacets | Returns or sets the option to identify or repair facets with with one long edge and two edges with more or the less the same length and a ratio of length to width exceeding a specified value |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
DisplayCleanupReportInListWindow | Displays the NXOpen.ListingWindow with numbers of various type of defects identified or repaired. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetAllOptionsToAnalyze | Sets all cleanup options to Facet.CleanupFacetBodyBuilderCleanupOptions.Analyze , which means to identify the defects only for the input bodies |
SetAllOptionsToNone | Sets all cleanup options to Facet.CleanupFacetBodyBuilderCleanupOptions.None , which means to do nothing |
SetAllOptionsToRepair | Sets all cleanup options to Facet.CleanupFacetBodyBuilderCleanupOptions.Repair , which means to identify as well as repair the defects for the input bodies |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CleanupFacetBodyBuilderCleanupOptions Enumeration | These represent the options for each facet defect |
CleanupFacetBodyBuilderOriginalBodyOptions Enumeration | These represent the options for handling the input bodies |
Property Detail¶
FoldedEdges¶
-
CleanupFacetBodyBuilder.
FoldedEdges
¶ Returns or sets the option to identify or repair facets having an angle with adjacent facets less than a specified minimum value
-------------------------------------
Getter Method
Signature
FoldedEdges()
Returns: Return type: NXOpen.Facet.CleanupFacetBodyBuilderCleanupOptions
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FoldedEdges(foldedEdges)
Parameters: foldedEdges ( NXOpen.Facet.CleanupFacetBodyBuilderCleanupOptions
) –New in version NX10.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
InconsistentNormals¶
-
CleanupFacetBodyBuilder.
InconsistentNormals
¶ Returns or sets the option to identify or repair normals of neighboring facets or vertices that do not have the right orientation
-------------------------------------
Getter Method
Signature
InconsistentNormals()
Returns: Return type: NXOpen.Facet.CleanupFacetBodyBuilderCleanupOptions
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InconsistentNormals(inconsistentNormals)
Parameters: inconsistentNormals ( NXOpen.Facet.CleanupFacetBodyBuilderCleanupOptions
) –New in version NX10.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
InputBodies¶
-
CleanupFacetBodyBuilder.
InputBodies
¶ Returns the input facet bodies to be analyzed or repaired
-------------------------------------
Getter Method
Signature
InputBodies()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX10.0.0.
License requirements: None.
LaminarSlits¶
-
CleanupFacetBodyBuilder.
LaminarSlits
¶ Returns or sets the option to identify or repair thin holes or slits in the mesh caused by facets not being aligned
-------------------------------------
Getter Method
Signature
LaminarSlits()
Returns: Return type: NXOpen.Facet.CleanupFacetBodyBuilderCleanupOptions
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LaminarSlits(laminarSlits)
Parameters: laminarSlits ( NXOpen.Facet.CleanupFacetBodyBuilderCleanupOptions
) –New in version NX10.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
LongFacets¶
-
CleanupFacetBodyBuilder.
LongFacets
¶ Returns or sets the option to identify or repair facets with a ratio of longest to shortest side exceeding a specified value
-------------------------------------
Getter Method
Signature
LongFacets()
Returns: Return type: NXOpen.Facet.CleanupFacetBodyBuilderCleanupOptions
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LongFacets(longFacets)
Parameters: longFacets ( NXOpen.Facet.CleanupFacetBodyBuilderCleanupOptions
) –New in version NX10.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
MaxRatioLongFacets¶
-
CleanupFacetBodyBuilder.
MaxRatioLongFacets
¶ Returns or sets the specified value used to define long facets
-------------------------------------
Getter Method
Signature
MaxRatioLongFacets()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaxRatioLongFacets(maxRatioLongFacets)
Parameters: maxRatioLongFacets (float) – New in version NX10.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
MinAngleFoldedFacets¶
-
CleanupFacetBodyBuilder.
MinAngleFoldedFacets
¶ Returns or sets the minimum angle between adjacent facets to define folded facets
-------------------------------------
Getter Method
Signature
MinAngleFoldedFacets()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinAngleFoldedFacets(minAngleFoldedFacets)
Parameters: minAngleFoldedFacets (float) – New in version NX10.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
OriginalBodyOption¶
-
CleanupFacetBodyBuilder.
OriginalBodyOption
¶ Returns or sets the option for handling the input facet bodies
-------------------------------------
Getter Method
Signature
OriginalBodyOption()
Returns: Return type: NXOpen.Facet.CleanupFacetBodyBuilderOriginalBodyOptions
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OriginalBodyOption(enumOriginalBodyOption)
Parameters: enumOriginalBodyOption ( NXOpen.Facet.CleanupFacetBodyBuilderOriginalBodyOptions
) –New in version NX11.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
SelfIntersections¶
-
CleanupFacetBodyBuilder.
SelfIntersections
¶ Returns or sets the option to identify or repair facets of the same mesh intersecting each other
-------------------------------------
Getter Method
Signature
SelfIntersections()
Returns: Return type: NXOpen.Facet.CleanupFacetBodyBuilderCleanupOptions
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelfIntersections(selfIntersections)
Parameters: selfIntersections ( NXOpen.Facet.CleanupFacetBodyBuilderCleanupOptions
) –New in version NX10.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ShowInfo¶
-
CleanupFacetBodyBuilder.
ShowInfo
¶ Returns or sets the option to display numbers of various type of defects identified or repaired in the
NXOpen.ListingWindow
.If this option is true, but the program is running externally without UI, display would go to a standard output devicethe. The listing window output can be sent to the Information window or to a file, or to both. See
NXOpen.ListingWindow.SelectDevice()
for more information.-------------------------------------
Getter Method
Signature
ShowInfo()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowInfo(showInfo)
Parameters: showInfo (bool) – New in version NX10.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ThinFacets¶
-
CleanupFacetBodyBuilder.
ThinFacets
¶ Returns or sets the option to identify or repair facets with with one long edge and two edges with more or the less the same length and a ratio of length to width exceeding a specified value
-------------------------------------
Getter Method
Signature
ThinFacets()
Returns: Return type: NXOpen.Facet.CleanupFacetBodyBuilderCleanupOptions
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ThinFacets(thinFacets)
Parameters: thinFacets ( NXOpen.Facet.CleanupFacetBodyBuilderCleanupOptions
) –New in version NX11.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Method Detail¶
DisplayCleanupReportInListWindow¶
-
CleanupFacetBodyBuilder.
DisplayCleanupReportInListWindow
¶ Displays the
NXOpen.ListingWindow
with numbers of various type of defects identified or repaired.If we call this method externally without UI, it displays the information on standard output device. The listing window output can be sent to the Information window or to a file, or to both. See
NXOpen.ListingWindow.SelectDevice()
for more information.Signature
DisplayCleanupReportInListWindow()
New in version NX11.0.0.
License requirements: None.
SetAllOptionsToAnalyze¶
-
CleanupFacetBodyBuilder.
SetAllOptionsToAnalyze
¶ Sets all cleanup options to
Facet.CleanupFacetBodyBuilderCleanupOptions.Analyze
, which means to identify the defects only for the input bodiesSignature
SetAllOptionsToAnalyze()
New in version NX10.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
SetAllOptionsToNone¶
-
CleanupFacetBodyBuilder.
SetAllOptionsToNone
¶ Sets all cleanup options to
Facet.CleanupFacetBodyBuilderCleanupOptions.None
, which means to do nothingSignature
SetAllOptionsToNone()
New in version NX10.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
SetAllOptionsToRepair¶
-
CleanupFacetBodyBuilder.
SetAllOptionsToRepair
¶ Sets all cleanup options to
Facet.CleanupFacetBodyBuilderCleanupOptions.Repair
, which means to identify as well as repair the defects for the input bodiesSignature
SetAllOptionsToRepair()
New in version NX10.0.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Validate¶
-
CleanupFacetBodyBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.