BestFitAlignBuilderConstraintOptions Enumeration

NXOpen.Facet.BestFitAlignBuilder.ConstraintOptions is an alias for NXOpen.Facet.BestFitAlignBuilderConstraintOptions

class NXOpen.Facet.BestFitAlignBuilderConstraintOptions

Bases: object

Represents the constraint options

Enum Members

Enum Member Enum Member Description
Free
No constraint
OnlyTranslation
Only translation
TranslationInPlane
Translation in the plane
TranslationAlongDirection
Translation along direction
OnlyRotation
Only rotation
RotationAroundPoint
Rotation around specific point
RotationAroundLine
Rotation around specific line
HoldToPlane
Moving in the plane
HoldToLine
Moving along the line
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.