WallMaterialType Enumeration¶
NXOpen.Display.Wall.MaterialType is an alias for NXOpen.Display.WallMaterialType
-
class
NXOpen.Display.
WallMaterialType
¶ Bases:
object
Defines the material characteristics of a stage wall.
Deprecated since version NX10.0.0: Use
NXOpen.Display.WallWallMaterialTextureType
instead.Enum Members
shadows. Use this to cast shadows onto a “virtual” background image of an environment. “
“Reflective”, ” The wall is reflective. For example, use this on- a “bottom” wall to display a shiny floor. “
- “Invisible”, ” The wall is not displayed. For example, use this
on all the walls except the “bottom” if you only need to display a floor. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.