TrueStudioCollection Class¶
-
class
NXOpen.Display.
TrueStudioCollection
¶ Bases:
object
Represents a collection TrueStudio objects
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreateTrueStudioBuilder | Creates a NXOpen.Display.TrueStudioBuilder object if TrueStudio is None. |
FindObject | Finds the NXOpen.Display.TrueStudio with the given identifier as recorded in a journal. |
Method Detail¶
CreateTrueStudioBuilder¶
-
TrueStudioCollection.
CreateTrueStudioBuilder
¶ Creates a
NXOpen.Display.TrueStudioBuilder
object if TrueStudio is None.Otherwise, a TrueStudio object will be edited
Signature
CreateTrueStudioBuilder(sObj)
Parameters: sObj ( NXOpen.Display.TrueStudio
) – If TrueStudio object is not None, then this object will be editedReturns: return TrueStudio object builder Return type: NXOpen.Display.TrueStudioBuilder
New in version NX6.0.0.
License requirements: None.
FindObject¶
-
TrueStudioCollection.
FindObject
¶ Finds the
NXOpen.Display.TrueStudio
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: TrueStudio object found Return type: NXOpen.Display.TrueStudio
New in version NX6.0.0.
License requirements: None.