TrueShadingBuilderSurfaceOrientType Enumeration¶
NXOpen.Display.TrueShadingBuilder.SurfaceOrientType is an alias for NXOpen.Display.TrueShadingBuilderSurfaceOrientType
-
class
NXOpen.Display.
TrueShadingBuilderSurfaceOrientType
¶ Bases:
object
Shadow plane projection orientation types
Enum Members
Enum Member Enum Member Description NotSet Do not project shadowsBottom Project shadows onto the floorBack Project shadows onto the back wallBottomFixed Project shadows onto a fixed oriented floor-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-