TrueShadingBuilderEnvironmentMapType Enumeration¶
NXOpen.Display.TrueShadingBuilder.EnvironmentMapType is an alias for NXOpen.Display.TrueShadingBuilderEnvironmentMapType
-
class
NXOpen.Display.
TrueShadingBuilderEnvironmentMapType
¶ Bases:
object
Global environment reflection map types
Enum Members
Enum Member Enum Member Description Default No reflection mapMetalShiny1 Shiny Metal Reflection 1MetalShiny2 Shiny Metal Reflection 2MetalBrushed1 Brushed Metal Reflection 1MetalBrushed2 Brushed Metal Reflection 2Glossy1 Glossy Reflection 1Glossy2 Glossy Reflection 2SurfaceAnalysisLines Surface Analysis Lines ReflectionSurfaceAnalysisHorizon Surface Analysis Horizontal Lines ReflectionAutoPhotoStudio Automotive Lighting ReflectionCustomImage Custom Image Reflection-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-