TrueShadingBuilderBgdType Enumeration¶
NXOpen.Display.TrueShadingBuilder.BgdType is an alias for NXOpen.Display.TrueShadingBuilderBgdType
-
class
NXOpen.Display.
TrueShadingBuilderBgdType
¶ Bases:
object
Background colors and image types
Enum Members
Enum Member Enum Member Description DarkGraduated Graduated dark colored backgroundLightGraduated Graduated light colored backgroundBlack Plain dark Colored backgroundWhite Plain light Colored backgroundCustomPlain Customized plain colored backgroundCustomGraduated Customized graduated colored backgroundInheritShadedBackground Use same background color as in shaded display modeImageBackground Use one of the predefined images as background-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-