TransientTextViewType Enumeration¶
NXOpen.Display.TransientText.ViewType is an alias for NXOpen.Display.TransientTextViewType
-
class
NXOpen.Display.
TransientTextViewType
¶ Bases:
object
the view or views in which the transient text is to be displayed.
Note that this property is only used when the view property is other than None.
Enum Members
Enum Member Enum Member Description WorkViewOnly AllActiveViews ViewOfLastCursor AllViewsButDrawing AllActiveMemberViews FirstViewFound -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-