StudioImageCaptureBuilderUnitsEnumType Enumeration¶
NXOpen.Display.StudioImageCaptureBuilder.UnitsEnumType is an alias for NXOpen.Display.StudioImageCaptureBuilderUnitsEnumType
-
class
NXOpen.Display.
StudioImageCaptureBuilderUnitsEnumType
¶ Bases:
object
Provide the following resolution unit options to screen capture
Enum Members
Enum Member Enum Member Description Pixels Use pixel to define resolutionMm Use Millimeters to define resolutionInches Use Inched to define resolution-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-