StudioImageCaptureBuilderOrientEnumType Enumeration¶
NXOpen.Display.StudioImageCaptureBuilder.OrientEnumType is an alias for NXOpen.Display.StudioImageCaptureBuilderOrientEnumType
-
class
NXOpen.Display.
StudioImageCaptureBuilderOrientEnumType
¶ Bases:
object
Provide the following options to image orientation
Enum Members
Enum Member Enum Member Description Landscape Capture image in landscape modePortrait Capture image in portrait mode-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-