StudioImageCaptureBuilderDrawingSizeEnumType Enumeration¶
NXOpen.Display.StudioImageCaptureBuilder.DrawingSizeEnumType is an alias for NXOpen.Display.StudioImageCaptureBuilderDrawingSizeEnumType
-
class
NXOpen.Display.
StudioImageCaptureBuilderDrawingSizeEnumType
¶ Bases:
object
Provide the following standard Drawing sizes
Enum Members
Enum Member Enum Member Description Isoa4 Use ISO A4 drawing sizeIsoa3 Use ISO A3 drawing sizeIsoa2 Use ISO A2 drawing sizeIsoa1 Use ISO A1 drawing sizeIsoa0 Use ISO A0 drawing sizeAnsia Use ANSI A drawing sizeAnsib Use ANSI B drawing sizeAnsic Use ANSI C drawing sizeAnsid Use ANSI D drawing sizeAnsie Use ANSI E drawing sizeCustom Use custom defined drawing size-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-