ShadowsRealTimeState Enumeration¶
NXOpen.Display.Shadows.RealTimeState is an alias for NXOpen.Display.ShadowsRealTimeState
-
class
NXOpen.Display.
ShadowsRealTimeState
¶ Bases:
object
Real time type settings - environment_shadow_catcher_only is enabled only in Basic Studio mode
Enum Members
Enum Member Enum Member Description Disabled Realtime is disabledEnvironmentShadowCatcherOnly Realtime Environment or shadow catcher onlyInterObject Realtime Inter-object shadows-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-