SelPrefMouseGesture Enumeration¶
NXOpen.Display.SelPref.MouseGesture is an alias for NXOpen.Display.SelPrefMouseGesture
-
class
NXOpen.Display.
SelPrefMouseGesture
¶ Bases:
object
Represents the mouse gesture type
Enum Members
Enum Member Enum Member Description Lasso multi-select using lassoRectangle multi-select using rectangleCircle multi-select using circle-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-