ReflectionType Enumeration¶
NXOpen.Display.Reflection.Type is an alias for NXOpen.Display.ReflectionType
-
class
NXOpen.Display.
ReflectionType
¶ Bases:
object
where the reflections for rendering will be obtained
Enum Members
Enum Member Enum Member Description Background use the background for reflectionsStage use the stage for reflectionsIbl use the image-based lighting image for reflectionsImage use the given image file for reflection-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-