RayTracedStudioEditorBuilderStaticRayTracedStudioQualityType Enumeration¶
NXOpen.Display.RayTracedStudioEditorBuilder.StaticRayTracedStudioQualityType is an alias for NXOpen.Display.RayTracedStudioEditorBuilderStaticRayTracedStudioQualityType
-
class
NXOpen.Display.
RayTracedStudioEditorBuilderStaticRayTracedStudioQualityType
¶ Bases:
object
To specify the quality and performance of the Ray Traced Studio display during static image rendering
Enum Members
Enum Member Enum Member Description High Very good ray traced display quality for static image renderingMedium Good quality ray traced display with good performance for static image renderingLow The fastest ray traced display performance with preview quality for static image renderingUserDefined User specified ray traced display quality for static image rendering-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-