RayTracedStudioEditorBuilderStaticAntialiasingType Enumeration¶
NXOpen.Display.RayTracedStudioEditorBuilder.StaticAntialiasingType is an alias for NXOpen.Display.RayTracedStudioEditorBuilderStaticAntialiasingType
-
class
NXOpen.Display.
RayTracedStudioEditorBuilderStaticAntialiasingType
¶ Bases:
object
To specify the antialiasing quality during stationary Ray Traced Studio display during static image rendering
Enum Members
Enum Member Enum Member Description High Very good antialiasing performed for static image renderingMedium Good antialiasing performed for static image renderingLow Coarse antialiasing performed for static image renderingNotSet No antialiasing performed to provide quick, preview of ray traced display for static image rendering-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-