RayTracedStudioEditorBuilderRayTracedStudioStaticImageUnitsType Enumeration¶
NXOpen.Display.RayTracedStudioEditorBuilder.RayTracedStudioStaticImageUnitsType is an alias for NXOpen.Display.RayTracedStudioEditorBuilderRayTracedStudioStaticImageUnitsType
-
class
NXOpen.Display.
RayTracedStudioEditorBuilderRayTracedStudioStaticImageUnitsType
¶ Bases:
object
To specify the Ray Traced Studio static image units
Enum Members
Enum Member Enum Member Description Pixels static image size specified in pixelMillimeters static image size specified in millimetersInches static image size specified in inches-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-