RayTracedStudioEditorBuilderDynamicRayTracedStudioTilingQualityType Enumeration¶
NXOpen.Display.RayTracedStudioEditorBuilder.DynamicRayTracedStudioTilingQualityType is an alias for NXOpen.Display.RayTracedStudioEditorBuilderDynamicRayTracedStudioTilingQualityType
-
class
NXOpen.Display.
RayTracedStudioEditorBuilderDynamicRayTracedStudioTilingQualityType
¶ Bases:
object
To specify the quality and performance of the interactive, dynamic Ray Traced Studio display.
Affects the number of tiles presented in the display.
Enum Members
Enum Member Enum Member Description High Very small tiles used during progressive updates of ray traced displayMedium Medium sized tiles used during progressive updates of ray traced displayLow Larger tiles used during progressive updates of ray traced display for faster display time-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-