PointCloudClippingBoxesListItemBuilder Class¶
-
class
NXOpen.Display.
PointCloudClippingBoxesListItemBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Display.PointCloudClippingBoxesListItemBuilder
to create clipping regions forNXOpen.Display.PointCloud
.To create a new instance of this class, use
NXOpen.Display.PointCloudBuilder.CreateClippingBoxesListItemBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ClippingEndPoint | Returns or sets the end point of the clipping box diagonal |
ClippingSide | Returns or sets the clipping side of the defined clipping box |
ClippingStartPoint | Returns or sets the start point of the clipping box diagonal. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PointCloudClippingBoxesListItemBuilderClippingSides Enumeration | Specifies clipping side options used for defined clipping box. |
Property Detail¶
ClippingEndPoint¶
-
PointCloudClippingBoxesListItemBuilder.
ClippingEndPoint
¶ Returns or sets the end point of the clipping box diagonal
-------------------------------------
Getter Method
Signature
ClippingEndPoint()
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClippingEndPoint(clippingEndPoint)
Parameters: clippingEndPoint ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_point_cloud_view (“NX Point Cloud Viewer”)
ClippingSide¶
-
PointCloudClippingBoxesListItemBuilder.
ClippingSide
¶ Returns or sets the clipping side of the defined clipping box
-------------------------------------
Getter Method
Signature
ClippingSide()
Returns: Return type: NXOpen.Display.PointCloudClippingBoxesListItemBuilderClippingSides
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClippingSide(clippingSide)
Parameters: clippingSide ( NXOpen.Display.PointCloudClippingBoxesListItemBuilderClippingSides
) –New in version NX11.0.0.
License requirements: nx_point_cloud_view (“NX Point Cloud Viewer”)
ClippingStartPoint¶
-
PointCloudClippingBoxesListItemBuilder.
ClippingStartPoint
¶ Returns or sets the start point of the clipping box diagonal.
-------------------------------------
Getter Method
Signature
ClippingStartPoint()
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClippingStartPoint(clippingStartPoint)
Parameters: clippingStartPoint ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_point_cloud_view (“NX Point Cloud Viewer”)
Method Detail¶
Validate¶
-
PointCloudClippingBoxesListItemBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.