PlaneGridBuilder Class¶
-
class
NXOpen.Display.
PlaneGridBuilder
¶ Bases:
NXOpen.Display.BoundedGridBuilder
Represents the builder for adding a bounded grid
NXOpen.Display.PlaneGrid
to a plane.To create a new instance of this class, use
NXOpen.Display.GridCollection.CreatePlaneGridBuilder()
Default values.
Property Value Associative 1 LabelReference Local MajorLineSpacing 100 (millimeters part), 1 (inches part) MajorLineStyle Solid MajorLineWeight Normal MinorLineStyle Dashed MinorLineWeight Thin MinorLinesPerMajor 1 Show 1 ShowLabel Always ShowMajorLines 1 ShowOnTop 0 SnapPointsPerMinor 1 SnapToGrid 0 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Associative | Returns or sets the associative |
LabelReference | Returns or sets the label reference |
LineColor | Returns or sets the line color |
LocalOrigin | Returns or sets the local origin |
MajorLineSpacing | Returns or sets the major line spacing |
MajorLineStyle | Returns or sets the major line style |
MajorLineWeight | Returns or sets the major line weight |
MinorLineStyle | Returns or sets the minor line style |
MinorLineWeight | Returns or sets the minor line weight |
MinorLinesPerMajor | Returns or sets the minor lines per major |
Plane | Returns or sets the plane |
SectionCurveSettings | Returns the curve settings builder |
Show | Returns or sets the show |
ShowLabel | Returns or sets the show labels |
ShowMajorLines | Returns or sets the show major lines |
ShowOnTop | Returns or sets the show on top |
SnapPointsPerMinor | Returns or sets the snap points per minor |
SnapToGrid | Returns or sets the snap to grid |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCornerPoints | Gets corner points of the grid @return Flag indicating whether the corner points are valid |
GetObject | Returns the object currently being edited by this builder. |
InheritSettings | Inherits the settings from the specified grid. |
SaveCurves | Creates curves by intersecting the bounded grid with all bodies in the part of the grid object. |
SetCornerPoints | Sets corner points of the grid @return Flag indicating whether the corner points are valid |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Plane¶
-
PlaneGridBuilder.
Plane
¶ Returns or sets the plane
-------------------------------------
Getter Method
Signature
Plane()
Returns: Return type: NXOpen.Plane
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Plane(plane)
Parameters: plane ( NXOpen.Plane
) –New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
PlaneGridBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.