ImageTestBuilderAttributeType Enumeration¶
NXOpen.Display.ImageTestBuilder.AttributeType is an alias for NXOpen.Display.ImageTestBuilderAttributeType
-
class
NXOpen.Display.
ImageTestBuilderAttributeType
¶ Bases:
object
Indicates the extra display attribute that is enabled for the display object (DISP_OBJ) that displays the image in the graphics window.
Enum Members
Enum Member Enum Member Description NotSet DeEmphasis ShowThrough Overlay -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-