ImageBaseBuilderSizeOptions Enumeration¶
NXOpen.Display.ImageBaseBuilder.SizeOptions is an alias for NXOpen.Display.ImageBaseBuilderSizeOptions
-
class
NXOpen.Display.
ImageBaseBuilderSizeOptions
¶ Bases:
object
Describes size options.
Enum Members
Enum Member Enum Member Description UserDefined user defined optionImageSize image size optionReferenceScaling reference scaling option-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-