IRayPlusStudioEditorBuilderIRayPlusStudioStaticImageResolutionType Enumeration¶
NXOpen.Display.IRayPlusStudioEditorBuilder.IRayPlusStudioStaticImageResolutionType is an alias for NXOpen.Display.IRayPlusStudioEditorBuilderIRayPlusStudioStaticImageResolutionType
-
class
NXOpen.Display.
IRayPlusStudioEditorBuilderIRayPlusStudioStaticImageResolutionType
¶ Bases:
object
To specify the Ray Traced Studio static image resolution
Enum Members
Enum Member Enum Member Description High static image output resolution of 300 DPI (dots per inch)Medium static image output resolution of 150 DPI (dots per inch)Low static image output resolution of 72 DPI (dots per inch)UserDefined user specified image output resolution in DPI (dots per inch)-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-