DynamicSectionTypesClip Enumeration¶
NXOpen.Display.DynamicSectionTypes.Clip is an alias for NXOpen.Display.DynamicSectionTypesClip
-
class
NXOpen.Display.
DynamicSectionTypesClip
¶ Bases:
object
Specifies clipping type.
The “Slice” type is only available for “One Plane” section. “Section” will clip data that lies on the opposite side of the plane normal of the clipping plane.
Enum Members
Enum Member Enum Member Description Section One sided clipSlice Slice type clip-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-