DynamicSectionTypesActivePlane Enumeration¶
NXOpen.Display.DynamicSectionTypes.ActivePlane is an alias for NXOpen.Display.DynamicSectionTypesActivePlane
-
class
NXOpen.Display.
DynamicSectionTypesActivePlane
¶ Bases:
object
Specifies active clip plane in the active plane pair.
This is used in “Two Parallel Planes” and “Box” type Sections.
Enum Members
Enum Member Enum Member Description Primary PrimarySecondary Secondary-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-