DecalCollection Class¶
-
class
NXOpen.Display.
DecalCollection
¶ Bases:
object
Represents a collection decal material texture
This class is restricted to being called from a program running during an Interactive NX session. If run from a non-interactive session it will return None.
To obtain an instance of this class, refer to
NXOpen.BasePart
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreateDecalBuilder | Creates a NXOpen.Display.DecalBuilder object if decal is None. |
CreateDecalBuilderFull | Creates a NXOpen.Display.DecalBuilder object with image referenced object if decal is None. |
FindDecalObject | Finds the NXOpen.Decal with the given identifier as recorded in a journal. |
Method Detail¶
CreateDecalBuilder¶
-
DecalCollection.
CreateDecalBuilder
¶ Creates a
NXOpen.Display.DecalBuilder
object if decal is None.Otherwise, a Decal object will be edited
Signature
CreateDecalBuilder(decal)
Parameters: decal ( NXOpen.TaggedObject
) – If decal is not None, then this object will be editedReturns: return decal builder Return type: NXOpen.Display.DecalBuilder
New in version NX6.0.0.
License requirements: None.
CreateDecalBuilderFull¶
-
DecalCollection.
CreateDecalBuilderFull
¶ Creates a
NXOpen.Display.DecalBuilder
object with image referenced object if decal is None.Otherwise, a Decal object will be edited
Signature
CreateDecalBuilderFull(decal)
Parameters: decal ( NXOpen.TaggedObject
) – If decal is not None, then this object will be editedReturns: return decal builder Return type: NXOpen.Display.DecalBuilder
New in version NX6.0.0.
License requirements: None.
FindDecalObject¶
-
DecalCollection.
FindDecalObject
¶ Finds the
NXOpen.Decal
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindDecalObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: Decal found Return type: NXOpen.Decal
New in version NX6.0.0.
License requirements: None.