DecalBuilderAnchor Enumeration¶
NXOpen.Display.DecalBuilder.Anchor is an alias for NXOpen.Display.DecalBuilderAnchor
-
class
NXOpen.Display.
DecalBuilderAnchor
¶ Bases:
object
image anchor
Enum Members
Enum Member Enum Member Description TopLeft anchor at top left corner of decal imageCenter anchor in the middle of decal imageBottomLeft anchor at the bottom left corner of decal imageTopMiddle anchor at top middle corner of decal imageTopRight anchor at top right corner of decal imageLeftMiddle anchor at left middle corner of decal imageRightMiddle anchor at right middle corner of decal imageBottomMiddle anchor at bottom middle corner of decal imageBottomRight anchor at bottom right corner of decal image-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-