DatumPlaneGridBuilderGridOrientationType Enumeration¶
NXOpen.Display.DatumPlaneGridBuilder.GridOrientationType is an alias for NXOpen.Display.DatumPlaneGridBuilderGridOrientationType
-
class
NXOpen.Display.
DatumPlaneGridBuilderGridOrientationType
¶ Bases:
object
Specifies grid orientation option to be used for grid display.
Enum Members
- datum plane display “
- “Custom”, ” Grid size, location, and
orientation can be customized using the manipulator controls “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.