CanonMRTestBuilderImageUsageType Enumeration¶
NXOpen.Display.CanonMRTestBuilder.ImageUsageType is an alias for NXOpen.Display.CanonMRTestBuilderImageUsageType
-
class
NXOpen.Display.
CanonMRTestBuilderImageUsageType
¶ Bases:
object
Indicates how the image identified by ImageFile is specified to CGP.
Enum Members
The image is ignored, so neither background nor foreground is displayed. “
“Dual”, “The image is specified as a dual image that is displayed as both the background and foreground. “
“Background3Only”, “The image is specified as a BGR or RGB background image only, so no foreground is displayed. “
“Background4Only”, “The image is specified as a BGRA or RGBA background image only, so no foreground is displayed. “
“Background3AndForeground”, “The image is specified separately as a BGR or RGB background image and a foreground image. “
“Background4AndForeground”, “The image is specified separately as a BGRA or RGBA background image and a foreground image. “
“ForegroundOnly”, “The image is specified as a foreground image only, so no background is displayed. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-